Cancel
Showing results for 
Search instead for 
Did you mean: 

Transition area machining at turbine blade

Pioneer
Pioneer

Hello colleagues,

I have faced with the problem of programming a path for a blade. I have no idea how to make a spiral path like this on the part. If you have any idea, please help me.

BR,

Roman

1234.png

 

 

11 REPLIES 11

Re: Transition area machining at turbine blade

Siemens Phenom Siemens Phenom
Siemens Phenom

See the attached part file. Is this what you are looking for? I used the new Variable Axis Guiding Curves operation.

 

The graphics in your picture make it difficult to see exactly what tool path you desire.

Re: Transition area machining at turbine blade

Pioneer
Pioneer

Jkane1, thank you for your fast reply.

I have special blade milling machine with 2 jaw chucks.

I need to machine platform and radious. I highlighted them in red colour. I need to find a method to create spiral path which cover platform and radious.

1.png2.png

Re: Transition area machining at turbine blade

Gears Phenom Gears Phenom
Gears Phenom

he probably wants spiral pattern to "open" blade and then helical stepovers to machine blade with full depth of the tool

This is what I see on pictures...

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Transition area machining at turbine blade

Pioneer
Pioneer

I want to have something like this...

(view in My Videos)

Re: Transition area machining at turbine blade

Pioneer
Pioneer

Your help is still needed. =)

Re: Transition area machining at turbine blade

Valued Contributor
Valued Contributor

Hello

 

Maybe this is an inspiration for you:

I deleted the radius around the blade. Removed the contour of the blade "Foot" and made it a little bit bigger in the outer range. 

After that you recreate the radius.

After this modifications i created an operation "VARIABLE_AXIS_GUIDING_CURVES" like Mr. Jkane1 some changes in the min/max Angle.

 

2018-06-04_23h03_14.png  

 

2018-06-04_22h45_08.png

 

2018-06-04_22h45_26.png

 

The only problem is you got a toolpath with no cutting material.

Maybe with "Edit Toolpath" you can trim this path to perfection.

 

Best Regards

 


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Re: Transition area machining at turbine blade

Pioneer
Pioneer

Thank you Bernhard,

I can't repeat your operation. =(

Is it any here the instruction how to use step-by-step Guiding Curves?

Re: Transition area machining at turbine blade

Pioneer
Pioneer
Jkane1, How did you create spiral path? =) When I repeat your example, I have got Zig strategy.

Re: Transition area machining at turbine blade

Siemens Phenom Siemens Phenom
Siemens Phenom

I also used Guiding Curves to create the path, and GC is still under development, so you may not have all the current functionality. What version of NX are you running?

Learn online





Solution Information