Cancel
Showing results for 
Search instead for 
Did you mean: 

Transitions between 5ax operations?

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

Is there a possibility or workaround to "connect" 5 ax operations (with the same tool) with paths along clearance geometry? Or is it possible it will be developed?

 

I know that in the end of operation we just retract spindle to some save position.

But you know...I think and customers too that it could save the time and why not when path is in the clearence geometry.

 

thank you for your reactions

 

j

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
2 REPLIES

Re: Transitions between 5ax operations?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In theory you could NOT do the retract, and use a generic motion op between them.

But then you are responsible to keep it up to date as the operations change.

 

I'm not sure if the "bounding box" (or whatever) clearance can be used to generate the desired moves between operations?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Transitions between 5ax operations?

Gears Phenom Gears Phenom
Gears Phenom

ofcourse,  it is working, but there is lots of work (remember start and end coordinates, creating paths)

transition2.jpg

 

 

 

 

 

 

But it would be great the paths would by generated by system and checked.

 

(For example planar operations dont work in multiple planes and you have to create multiple operations.

These transitions would improve it in some way.)

 

 

thx

 

j

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information