Cancel
Showing results for 
Search instead for 
Did you mean: 

Tube rough test

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

Ive tested this operation with default setting:

 

It seems that in first level the cut depth is much bigger:

Snímka.JPG

The same result  was with 3D containment.

Any idea?

 

 

in Tube finish is ok:

Snímka2.JPG

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
7 REPLIES 7

Re: Tube rough test

Legend
Legend

did you enable Roll Tool Over Edges option in cutting parameters?

 

tube_machining__.JPG

If you want to avoid tool rolling over edges I think you have to extend tube surface as explained in the documentation:

tube_machining_0.JPG

 

extend Central curve too.

 

tube_machining_1.JPGtube_machining_2.JPG

 

ciao

Re: Tube rough test

Gears Phenom Gears Phenom
Gears Phenom

yes, I extended central curve and I have  extended surface a little.

 

But tube rough should compute path with IPW so result is wrong in this case I think.

To do workaround for machining the ipw is not good solution.

Only in case if this operation doesnt support IPW for generating paths.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Tube rough test

Legend
Legend

have you tried using 3d IPW in containment?

tube_machining_3.JPG

that should contain extended toolpath to ipw

tube_machining_4.JPG

 

Re: Tube rough test

Gears Phenom Gears Phenom
Gears Phenom

I tried it again and it is much better, but I had to use roll over the edges.

Snímka.JPG

 

Without roll over edges:

asd.JPG

(3D containment is turned on.)

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Tube rough test

Siemens Legend Siemens Legend
Siemens Legend

Dear Juraj,

 

I am interested to know if you think that the results after implementing the suggested workflow are satisfactory, or there are still open issues.

on the usability side - we have an enhancement request to address it in a more automatic way, but if we do that - we are leaving behind other things, so I am also interested on the priority of automatic path extension based on the IPW. what do you think?

 

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Tube rough test

Gears Phenom Gears Phenom
Gears Phenom

Hello Eddy,

 

I just thought that when I turn on the 3D containment the tool path will be automatically extended (like cavity mill etc) and I thought that it was a bug.

I dont now what everything else is behind this. I just did some tests.

 

To be honest I used once tube finishing but I did roughing by pre-drilling, hole milling and cavity milling (polycarbonate).

I am little bit afraid of using tube rough with lollypop tool for roughing (rigidity and time)

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Tube rough test

Siemens Legend Siemens Legend
Siemens Legend

Thanks Juraj for your prompt responseSmiley Happy

Turning on the 3D containment option would only contain the tool path to all locations where the tool is in contact with the In Process Workpiece (IPW) to prevent air cutting. In order to add moves you have to extend the coverage using a different method.

 

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Learn online





Solution Information