Cancel
Showing results for 
Search instead for 
Did you mean: 

[Turning] chamfer tool path

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi~

 

## Information

1. Version : NX11.0.2

2. Operation : Finish Turn OD

 

I have a question.

operation.jpg

 

The toolpath is 2 lines. The toolpath is offset and is created as a round in the corner.

 

round_path.jpg

 

 I set the Corners option to Extend. But it did not change.

 

cutting_parameter.jpg

 

I do not want to be output in rounds. I do not know if it is possible.

How do I set it up if possible?

 

1 REPLY 1

Re: [Turning] chamfer tool path

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would suggest reporting this to GTAC

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information