Cancel
Showing results for 
Search instead for 
Did you mean: 

Turning scenarios with rotary axis in the kinematic model are not supported in Tool Path simulation

Valued Contributor
Valued Contributor

Hello!

 

We have a MillTurn-Machine with rotary axis, it's a Mazak 1060. If I want to start Tool Path simulation (not NC-Code-Simulation) I get the message "Turning scenarios with rotary axis in the kinematic model are not supported in Tool Path simulation". Do I really need a NC-Code-based simulation (CSE, ...) ? 

 

2017-12-04 14_55_46-NX 10 - Fertigung - [cam_maz1060o_setup01_0].png

 

Can that be true? We live in 2017 and I use NX12.

 

Werner

 

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk

Learn online





Solution Information