Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: UDE List in NX9 is incorrect in one part but fine in others

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The null machine was the problem, since it is actually a machine with its own CDL file.

 

Starting with NX 8 you no longer need a null machine and it was bad practice in the past.

There is now the ability to remove a machine and get back to the default setup starting with NX 8.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
Highlighted

Re: UDE List in NX9 is incorrect in one part but fine in others

Randy,

Glad to see you have a "solution".

 

It was not the setup libray or configuration - I think you are correct about the machine tool.

We added the command to Remove Machine, which makes it GENERIC_MACHINE..

Prior to that you had to replace the machine with the NULL machine, but it was not the same as never having had a machine.

So perhaps the fact that there is a machine present (even a NULL machine) has something to do with it. 

Mark Rief
Retired Siemens

Learn online





Solution Information