Cancel
Showing results for 
Search instead for 
Did you mean: 

UDE markers

Gears Phenom Gears Phenom
Gears Phenom

Hello guys,

 

could somebody please explain me what UDEs :

Gohome_marker, return_marker, approach_marker_from_marker, start_marker, spindle_marker do?

 

When I am doind debug there is no extra event with using them.

What is their purpose?

 

Thank you

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
3 REPLIES

Re: UDE markers

Legend
Legend
This marker defines when the Output of your UDE is written zo the NC-File.

For example if you call an UDE in Start of Operation
Your_UDE
Than the Output is in Start_of_path

if you use an Marker
approach_marker
Your_UDE
Than the output of your UDE is written after the aproach_move (first move in the operation)


Re: UDE markers

Gears Phenom Gears Phenom
Gears Phenom
The markers are supposed to control when another UDE is output.
For example
You want the coolant to come on after the tool reaches the Z depth but before it starts cutting.
Use the approach marker and then the coolant on

others only work when the corresponding move is active. Start, Gohome, Return are moves you can find under the non cutting moves - Avoidance
so if you have defined a Return point you could add a UDE to output before or after the return point.

The spindle marker controls when the spindle code is output.

However depending on how the post is set up some of these do nothing.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: UDE markers

Gears Phenom Gears Phenom
Gears Phenom

@joycejo@schauerm3

 

thank you for explanation

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information