Cancel
Showing results for 
Search instead for 
Did you mean: 

UV Coordinates Wirecut have problem

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello all,

Anybody please help why UV coordinate very difference between Mitsubishi Wire cut EDM and Standard NX post for Mitsubishi as below:

 

Manufacturing cone shape: D1=10mm, D2=5mm

Untitled.png

 

Mitsubishi Gcode output:

G41G01X5.Y0.U5.V0.H1
G01X4.998Y0.14U-0.002V0.14
G01X4.992Y0.28U-0.006V0.141
G01X4.982Y0.42U-0.009V0.14
G01X4.969Y0.56U-0.015V0.139
G01X4.951Y0.699U-0.017V0.139
G01X4.929Y0.838U-0.021V0.138
G01X4.904Y0.975U-0.026V0.139
G01X4.875Y1.113U-0.03V0.136
G01X4.842Y1.249U-0.033V0.137
G01X4.805Y1.384U-0.037V0.135

 This is code output from NX

G41G01X5.Y0.0U-2.5V0.0F0.0
Y.057V-.028
X4.999Y.114U-2.499V-.057
X4.997Y.171V-.085
X4.995Y.228U-2.497V-.114
X4.992Y.286U-2.496V-.143
X4.988Y.344U-2.494V-.172
X4.984Y.402U-2.492V-.201
X4.978Y.461U-2.489V-.23
X4.973Y.519U-2.486V-.26
X4.966Y.578U-2.483V-.289
X4.959Y.637U-2.479V-.318
X4.951Y.696U-2.475V-.348

I imported this code to Mitsubishi Wire cut machine, the shape is not correct.

 

3 REPLIES 3

Re: UV Coordinates Wirecut have problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Looks liek NX is outputting UV in absolute values, Mitsubishi is expecting it to be incremental values (i.e. delta from XY position)

I've not touched Wire EDM posts in a while, there (hopefully) is an option to switch them, otherwise you'll have to figure out the math & change value to $upper(n) - $mom_pos(n)

(not sure the variable for "upper", but it should be the variable currently in the U/V words)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: UV Coordinates Wirecut have problem

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thanks Ken_A,

I will research

Re: UV Coordinates Wirecut have problem

Experimenter
Experimenter

I know your question , UG exprot the uv value, it is coordinate on upper, makino or sodick machine export nc from shapes ,like curves coordinate.good luck

Learn online





Solution Information