Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to edit cutting condition library NX12.0.1

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello ,
after installing the MP02 package for NX12.0.1, I do not have the ability to edit the cutting condition library. When clicked to edit the cutting condition library, the message pops up (see attachment).
Would anyone advise where the bug is?

Thank you

 

screen.PNG

2 REPLIES 2

Re: Unable to edit cutting condition library NX12.0.1

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

It seems to be a problem in MP2 and there is already a PR (9187856) for that in GTAC.

 

Greetings,

André 

Re: Unable to edit cutting condition library NX12.0.1

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

As mentioned there is a PR and development is working on a solution.

In the meantime you can try a workaround by adding below line into your local machining_data.tcl file.

 

 

set dbc_tc_library 0

 

 

Learn online





Solution Information