Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to open Inventor

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I have encouter an error when open invertor file. Does NX not able to open inventor file or there is another way to open inventor file?

Capture.PNG

 

2 REPLIES 2

Re: Unable to open Inventor

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Scooby_Doo ,

 

there is no direct exchange. I would do it with JT, Parasolid (if Inventor has that) or STEP. In that order ;-)

 

This topic might be interesting as well, as your next question possibly is why you can only see the Solid Model.

 

Files from Inventor

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: Unable to open Inventor

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi @AlexanderFreund,

 

It is fine that when open Inventor file(in STEP) in NX will result only in Solid Model. In fact, this is the result that we want just that needed to open Inverter file directly in NX without change the file to STEP file first.

 

Futhermore, is there any reason why NX could not open Inventer file directly? As by using Solid Edge 2019 (with Autodesk Inventer View 2019 install), it can be open inventer file directly. 

Learn online





Solution Information