Cancel
Showing results for 
Search instead for 
Did you mean: 

Using Floor / Wall

Experimenter
Experimenter
what better operation to machine the bottom radius ?

problem.jpg

I 'm using the operation floor / wall but does not eliminate the radius..I need help!!!
5 REPLIES 5

Re: Using Floor / Wall

Innovator
Innovator

Sinker EDM..

Proud Member Of The Reality-Based Community.

Re: Using Floor / Wall

Can you pick the floor as cut area and use area milling?

Mark Rief
Retired Siemens
Highlighted

Re: Using Floor / Wall

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have to machine the geometry *exactly* as in the picture, you will need to come at it from the side with a T cutter. (you can rough like you have it, but nothing other than T cutting or the sinker EDM option will cut the geometry *as shown*)

 

If you are allowed fillets in the corners, then bull-nose mill the "flat" section then use a ball nose cutter and surface contouring on the radius.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Using Floor / Wall

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And looking at it closer, a T cutter may not even fit (as the radius appears a bit small, there's probably no clearance for any realistic shank)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Using Floor / Wall

Innovator
Innovator

 


@Ken_A wrote:

And looking at it closer, a T cutter may not even fit (as the radius appears a bit small, there's probably no clearance for any realistic shank)


Sinker EDM.

Proud Member Of The Reality-Based Community.

Learn online





Solution Information