Cancel
Showing results for 
Search instead for 
Did you mean: 

Using machine tool bulder with any CAM set part file

Valued Contributor
Valued Contributor

hello dear friends.i have came acros some intresting case in my studies of NX.i have a fuly defined machine inside machine tool builder but with a seperate postprocesor for it.

here's a view of the machine inside machine tool builder

2019-01-21_193501.jpg 

I was wondering what is the sequence if it exsists to use this machine with any CAM setup part file in few simple steps whitout the need to define the machine in the machine library of NX and so on and so on.again if there's a way

 

thanks in advance.

3 REPLIES 3

Re: Using machine tool bulder with any CAM set part file

Legend
Legend

Well you could copy the machine and just change the script for the post it uses.

You could post your program using the post of your choice and run "simulate external code"?

 

If I have a machine loaded. I can use the post look-up to post with another post.

Then load...what I have just posted in machine simulate with "external program simulation".

I've done this to see what other post may do.

 

Not sure how you would load a machines common simulation engine (CSE) manually.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Highlighted

Re: Using machine tool bulder with any CAM set part file

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Aleitin

You could make a small customization/journal and assign it to a button on your tool bar. That would be a one push solution then. 

Regards

Paul

Re: Using machine tool bulder with any CAM set part file

Siemens Phenom Siemens Phenom
Siemens Phenom

The script might help.

 

What about adding this one time to the library and then create one CAM template part file with this machine tool assigned.

Each time doing a file new choice that template.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information