Cancel
Showing results for 
Search instead for 
Did you mean: 

Using modeling expressions in operations?

Legend
Legend
Has anyone requested this enhancement as explained below? Is there any plan to intoduce this in future NX versiosn? In Modeling, define expressions and use it in Machining operations.. e.g. Cylinder_Diameter=100mm Cylinder_Length=Cylinder_Diameter*1.5 Cutter_Diameter = Cylinder_Diameter*0.1 Then use 'Cutter_Diameter' expression from modeling to define cutter diameter.
2 REPLIES 2

Re: Using modeling expressions in operations?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

see

https://community.plm.automation.siemens.com/t5/Discussion-Forum-NX/Expressions-in-CAM/m-p/318691/hi...

 

Note as there's thousands (if not tens of thousands) of posisble places, Siemens would appreciate it if you could indicate the ones you are interested in.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Using modeling expressions in operations?

I am interested in the most common cases where you would use these.

 

For example, in your case above, we would probably recommend FBM to select the tool. 

Mark Rief
Retired Siemens

Learn online





Solution Information