Cancel
Showing results for 
Search instead for 
Did you mean: 

Using the faceted body as a blank

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I want to use faceted body as a blank in the "Simulate Machine Code File". The CAM project in the "Machine Tool Navigator" I ask "PART" - a solid model part, "FIXTURE" - model fixture solid and "BLANK" - FACETED body.
When I run the "Simulate Machine Code File" and turn on "Show 3D Material Removal" does not create a blank facet of body

What is the problem? It works or not?
When "Simulate Tool Path" blank facet of the body is created

 

6 REPLIES 6

Re: Using the faceted body as a blank

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I use in this case STL as PART, not as WORKPIECE. And for simulation I use blank as offset from PART:

 

 

Re: Using the faceted body as a blank

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I have tried is not working.It displays an error.
What am I doing
1) import STL model
2) Install the STL model as PART in Machine Tool Navigator
3) Run the simulation program file
4) include the Show 3D Material Removal and get an error

 

Re: Using the faceted body as a blank

Siemens Phenom Siemens Phenom
Siemens Phenom

For Material Removal in ISV "NC Code Simulation" a solid object is needed as initial blank input. faceted objects are not supported.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Using the faceted body as a blank

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

My fault, I import STL, but not change solid->stl.

another way - convert stl to solid body.

Re: Using the faceted body as a blank

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

What is the difference when using a facet body as a blank when simulating toolpaths and simulation program from a file?
When using the facet body as a blank during toolpath simulation everything works fine.

Re: Using the faceted body as a blank

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

50% or more of my clients want to use the ISV for simulating NC program files without having CAM processing project. There ISV model of the machine tool, the program file fixture model, the model parts and model of the workpiece facet body, just be able to use the scanned workpiece (STL).

Learn online





Solution Information