cancel
Showing results for 
Search instead for 
Did you mean: 

VNCK

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

When using VNCK for simulation in NX is it possible to use or import an NC file from another CAM system?

2 REPLIES

The Machine Simulation in NX can be set up as G-code driv...

Community Manager Community Manager
Community Manager

The Machine Simulation in NX can be set up as G-code driven simulation, which means that it takes as input the posted code that will actually go to the machine tool.  So yes, G code from any CAM system can be used to drive the Simulation in NX CAM. 

 

The Virtual NC Kernal (VNCK) is a particular optional component of Machine Simulation, with which it is possible to plug in the actual Sinumerik controller software as a black box machine driver.  Machine tool builders sometimes use this capability to create very accurate simulations, even including the Controller interface.  VNCK is not required for G code-driven machine tool simulation and is not typically used by most customers.  It is typically used by machine tool builders, as described.

Derek Hart
... if we're not having fun, we're not doing it right!

Re: The Machine Simulation in NX can be set up as G-code driv...

PLM World Member Creator PLM World Member Creator
PLM World Member Creator
Is it possible for the end user to get the VNCK from the machine and then apply it to ISV in NX?

-Danny

Learn online





Solution Information