Cancel
Showing results for 
Search instead for 
Did you mean: 

Variable contour error during surface selection for the drive geometry

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi, 

 

1. Anyone faced below issue when using the variable contour when selecting the surface selection for the drive goemetry?  What is the issue that causing it?

Capture2.PNG

 

Thank you.

3 REPLIES 3

Re: Variable contour error during surface selection for the drive geometry

Legend
Legend

Non-native geometry and the model rounds aren't necessarily the best in the industry. Best approach, and to machine this with NX's ootb toolpaths, you'll need to add new geometry. Lots of work ahead. Good luck.

 

00.jpg

 

01.jpg

 

Also, this option might be of use to you if you have many parts to make: 

https://www.youtube.com/watch?v=KjcYpjKdwDE

Re: Variable contour error during surface selection for the drive geometry

Siemens Phenom Siemens Phenom
Siemens Phenom

Have you tried guided curve...

 

ScreenHunter 85.png

Re: Variable contour error during surface selection for the drive geometry

Siemens Phenom Siemens Phenom
Siemens Phenom

Create a supplimentary swept surface to use as your Drive Geometry.

Capture19.JPG

The part file is attached.

 

Also, you may want to consider creating patch surfaces over the holes and an extension surface on the round edge to use in the defined Cut Area.

Learn online





Solution Information