Cancel
Showing results for 
Search instead for 
Did you mean: 

Variables for Diameter in Hole_Milling Operation

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Why can I not get the variables of the Feature, hole diameter and depth, in Hole_Making operation?  I have tried the Review Tool and Moog_show_variables.  Neither has shown them.  

Jeff Sauers, Lead CNC Programmer, Oberg Industries

Production: NX 10.0.3.5, Vericut 8.0


2 REPLIES

Re: Variables for Diameter in Hole_Milling Operation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Because NX does not export them to MOM.

See thread http://community.plm.automation.siemens.com/t5/Discussion-Forum-NX/Feature-parameters-for-Postproces...

 

If you want them, log an IR/ER

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Variables for Diameter in Hole_Milling Operation

Valued Contributor
Valued Contributor

Hello Jeff,

 

I'm also very interested to get this feature-parameters as mom-Variables in the Post. I've created an Enhancement Request for it: ER7328854

 

It would be helpful if you support this ER if you write to GTAC and make reference to my ER.

I think it should be possible for SPLM to do this.

 

Best regards

 

Werner

Werner
Production: NX10.0.3, FBM | TcUA 10.1.2.2
Development: VB.NET, Tcl/Tk | Testing: NX12.0

Learn online





Solution Information