Cancel
Showing results for 
Search instead for 
Did you mean: 

Verification missing gouge between toolholder and check surface

Phenom
Phenom

The help file isn't 100% definitive on this: is 3D verification supposed to spot gouges between holder and check surface? In my case it doesn't. I'm on CAM Express so I don't have the luxury of machine simulation. Gouge.JPGGouge2.JPG

2 REPLIES

Re: Verification missing gouge between toolholder and check surface

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello hjoy,

 

thanks for the question. 

 

I had a look in CAM Express 11 and I can see that option:

 

2017-09-11 09_16_08-Tool Path Visualization.png2017-09-11 09_16_57-Collision Settings.png

 

So it should do it.

 

Would you mind uploading the part, so I can check?

Lead Product Manager - Mold & Die

Re: Verification missing gouge between toolholder and check surface

Phenom
Phenom

Thanks Alexander,

 

I do have those same options ticked.. I'm sorry I can't post the part. If I have some spare time, I'll knock up a mockup and post that..

 

Learn online





Solution Information