Cancel
Showing results for 
Search instead for 
Did you mean: 

Verify Tool Path Layer

Valued Contributor
Valued Contributor

So I am working with legacy files from other programmers and trying to run Verify Tool Path on existing paths. The programmers and I use Model Views and Layer Visible In View to control visibility.

 

My question is why is the Verify Tool Path tool and path display set to a layer and how do you change this? For example, I have geometry on layers 30-40 for an operation butfor the toolpath to display and verify I have to make layer 70 visible to see it.

 

Thanks,

-Pat

6 REPLIES 6

Re: Verify Tool Path Layer

The path does not have a layer. In some cases, solid tool asemblies can have a layer. 

Are you saying the tool path is not visible if certain layers are off? If so, please provide some more information, or contact GTAC.

Mark Rief
Retired Siemens

Re: Verify Tool Path Layer

Legend
Legend
Try doing a file>utilities>part cleanup. Select 'clean manufacturing objects.' Backup your file 1st.
Glenn Balon
Production: NX 12.0.2 MP5 Primarily CAM

Re: Verify Tool Path Layer

Valued Contributor
Valued Contributor

Hey Mark,

 

I found out what the issue is. The video ink below explains what I found. It turns out that the Work Layer was not visible in Layer Visible in View. Let me know if you think this is working as advertised or I should report an IR.

 

https://www.screencast.com/t/loczQwFFbXQj

 

Once I get this project done I will be asking a lot of customization questions to write a C# app to capture and restore work/display states, that is if the API is deep enough to allow that. In my opinion there is a more efficient workflow than NX provides out of the box.

 

Thanks for your help!

 

 

Re: Verify Tool Path Layer

That sounds like it is working as expected. Having the work layer invisible means you do not want to see anything created, and that must include temporary display. 

Mark Rief
Retired Siemens

Re: Verify Tool Path Layer

Valued Contributor
Valued Contributor

I agree that appears to be the logic behind how it works but I don't think toolpath display should be associated with layer display as you stated in your first response to my initial question.

 

I will submit an IR with hopes it gets an ER.

 

Thanks!

Re: Verify Tool Path Layer

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
Try to avoid the use of layer-visible-in-view. This function only makes sense in drafting. In every other application it's a big annoyance.
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Learn online





Solution Information