Cancel
Showing results for 
Search instead for 
Did you mean: 

Verify Tool Path speed in NX10

Builder
Builder

Hello, verification tool path (2D or 3D) in NX10 for same parts is slower than NX9 or NX8.5.

It is possible to adjust setting for better speed visualisation?

Thanks.

4 REPLIES 4

Re: Verify Tool Path speed in NX10

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

The replay speed is not consistant.  Many times the speed of 1 is still too fast

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race
Highlighted

Re: Verify Tool Path speed in NX10

In 3D, how much difference are you seeing? 

What version are you running?

Mark Rief
Retired Siemens

Re: Verify Tool Path speed in NX10

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Mark,

 

We are running NX 10.0.3.5

I see at least a 50% difference.  For example with the Tool Path Visualization tab set to 3D Dynamic and the animation slider at 5 it is twice as fast as just the Reply tab.  The replay mode is not consistant IMHO.  I even wish I could slow it down even more sometimes! ( bet you never thought we would say that)

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Verify Tool Path speed in NX10

Builder
Builder

See attached files for comparison. Same parts, visualisation time in NX10 is cca 2x - 3x longer.

Please test prt files (same zoom in NX for test).

Learn online





Solution Information