Cancel
Showing results for 
Search instead for 
Did you mean: 

Verify Tool Path

Valued Contributor
Valued Contributor

When trying to use Verify Tool Path, the TABS, 3D Dynamic and 2D Dynamic are grayed out (unselected).

Also Display Options 2D Material Removal and show Previous IPW are not selectable.

 

It dose save IPW file both part file and part file with tool name extension add to part name, the file has data, but when you open them there is no geometry.

 

Do you need a license for this to work. I looked into this in NX10 documentation  and shows only ISV and Machine Vision needing a special License.

EDS UG V3 -UG V15 UNIX; UGS UG V6 -UG V19 - NX-NX5 UNIX/MS;
Siemens NX6-NX10; NX11; NX12; NX1847~Infinity MS
3 REPLIES 3

Re: Verify Tool Path

In the geometry view, is there a blank defined in the parent branch? - ususally this is in WORKPIECE.

 

What type of operation?

Mark Rief
Retired Siemens

Re: Verify Tool Path

Legend
Legend

Does the operation have a valid tool path?

Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5

Re: Verify Tool Path

Valued Contributor
Valued Contributor

 

Yes I have defined the blank. Have processed with collision and non-collision settings

 

The operations planner milling were generated and code posted the job has already ran across the machines.

 

I am using the file to learn and set up IPW process in company data base.

 

I will get with GTAC to work this out.

 

NX9.0.2.5

EDS UG V3 -UG V15 UNIX; UGS UG V6 -UG V19 - NX-NX5 UNIX/MS;
Siemens NX6-NX10; NX11; NX12; NX1847~Infinity MS

Learn online





Solution Information