Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

WARNING: unable to determine valid rotary positions__ in 4 axis mill table

Creator
Creator

Hi all,


I'm using 4 axis mill table with Sinumerik 840.
I want to drill 4 holes in my item (please see the attachment).


I am using only one origin (say G54) as local offset fixing for all the 4 holes.
When I pp the cycle, the output is right for the first three holes in Z+ direction, but I have a warning message "WARNING: unable to determine valid rotary positions" for the hole in X+ direction and the coordinates output are not listed.
Any suggestions?


Thanks in advance


SR


NX 10.0.2 MP4
PB 10.0.2

6 REPLIES 6

Re: WARNING: unable to determine valid rotary positions__ in 4 axis mill table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Guessing....

The one hole is SLIGHTLY angled is a direction the 4th axis can't get to.

List the internal toolpath and see if one of the tool axes has a non-zero small value in an "odd" direction

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: WARNING: unable to determine valid rotary positions__ in 4 axis mill table

Creator
Creator

It seems strange, but if I add another origin (say G55 example) that points the Z+ along the hole axis, the operation is ok without warnings.

 

SR

 

 

Re: WARNING: unable to determine valid rotary positions__ in 4 axis mill table

Legend
Legend

Check yout 'tool axis' in drilling operation and the way ypu select the holes.

Re: WARNING: unable to determine valid rotary positions__ in 4 axis mill table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'd look at the G55 MCS and check out its definition matrix.

I still think the hole is *just slightly* not square to the original MCS.

 

Again, in the internal toolpath, instead of

......,1, 0, 0

for the tool axis, you would see

....,.999999999, 0, .000000003

 

or whatever.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: WARNING: unable to determine valid rotary positions__ in 4 axis mill table

Creator
Creator

Thanks for the replies...


after many many attempts, I figured out that the problem is my machine's kinematics. In fact if I simulate the tool path with, for example sim03_mill_4ax in the installed machine example with its post-proc, the output is ok in any conditions.


I think that there are some problems in the machine's kinematics configuration that I created...

 

SR

 

 

 

 

 

Re: WARNING: unable to determine valid rotary positions__ in 4 axis mill table

Creator
Creator

Solved!

 

I was wrong to setting the spindle as a NC axis and so the machine is 5 axis instead of 4 axis.

 

SR

Learn online





Solution Information