Cancel
Showing results for 
Search instead for 
Did you mean: 

Want unlimited shank segments on tools????

Phenom
Phenom

multiple shanks.png

 

To show how many people may find this usefull. The more users who file an IR and link to this ER the better, to show it is needed.

 

Text in next line is from @Mould_United.

 

ER, # 9262232, asking for neck diameter definition which would allow us to define a shanked tool with a reduced neck diameter.

 

https://community.plm.automation.siemens.com/t5/Discussion-Forum-NX-Manufacturing/Relieved-Tools/m-p...

 

 

 

 

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM
39 REPLIES 39

Re: Want unlimited shank segments on tools?

Legend
Legend

Bump

 


Dennis Rathi
Creations Unlimited

Re: Want unlimited shank segments on tools?

Pioneer
Pioneer
What about Mill User Tool? You can define any tool profile, and set cutting length?

Re: Want unlimited shank segments on tools?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

With how many milling processors can you use MILL_USER_DEFINED?

Because I guess only with couple of them, which doesn't make it too useful

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Want unlimited shank segments on tools?

Phenom
Phenom

User defined does not work on all operations, and will not output parameters for tool lists. It's also much more time consuming to key in the information. New users always seem to struggle with it too. 

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: Want unlimited shank segments on tools????

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note (with some limitations) Step drills can also be used, and step drills can be used in most operation types (at least the ones I have tested)

But still a PITA to define the tool.

And there are some tools you have to use workarounds for.

Multiple shank segments would still be a better option (plus, then NX knows what is shank and what is cutting tool)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Want unlimited shank segments on tools????

Legend
Legend

Kirk:  I need more shank Scottie!!!

 

Scottie: I'm giving her all I've Got!!

 

need more shank.JPG

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Want unlimited shank segments on tools????

Phenom
Phenom

Walken-Cowbell_DS.jpg

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: Want unlimited shank segments on tools????

Legend
Legend

Bump... Smiley Wink

 


Dennis Rathi
Creations Unlimited

Re: Want unlimited shank segments on tools????

Phenom
Phenom

Bump!!!!!!!!!!!

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Learn online





Solution Information