Cancel
Showing results for 
Search instead for 
Did you mean: 

Waterjet with NX?

Gears Phenom Gears Phenom
Gears Phenom

NX 9, Tc 10

 

I don't see a water jet option, but NX will do wire edm.  

 

Is it possible to use the wire edm package, to program for a water jet?

 

Has anyone done this successfully?

 

How about nesting parts? 

 

Thanks,

 Dave

 

 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
3 REPLIES

Re: Waterjet with NX?

Legend
Legend

Hello

 

I have done such a machine with normal 3-5-axis milling operations. Also ther is a Post and CSE-Simulation for this machine

http://www.waterjet-ridder.com/en_waricut_hwe_3020_2_2d.php

 

 

 

Re: Waterjet with NX?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I have a postprocessor for ABB WaterJet robot. All toolpath from NX CAM - PLANAR, FIXED, VARIABLE. I have one interesting feature, may be will be interesting for you - I can calc thickness of material under jet and change robot velocity as function of thickness..

Re: Waterjet with NX?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I have ABB Water Jet robot. NX CAM for toolpath generation, PLANAR, FIXED, VARIABLE..

I have some interesting feature in my post - I can calc robot velocity depends on material thickness..

 

 

Learn online





Solution Information