Cancel
Showing results for 
Search instead for 
Did you mean: 

We are trying to simulate a 2ax fanuc lathe with ISV

Experimenter
Experimenter

We are trying to simulate a 2ax fanuc lathe with ISV and have tried using the files that came loaded with NX as a template but the template does not run a standard Fanuc turning program. The supplied files will only tool change when an M06 is called using Txx Hxx as the tool format. A Fanuc turning program does not run this way as it uses Txxxx without an M06. Also when making a return home move the fanuc lathe program uses G28 U0 W0 rather than use X0 and W0. the standard 2ax Fanuc machine will not recognise the U and W either.

 

Any tips on how to get this program to run?

 

(We are Running NX8.0)

1 REPLY 1

The simplest way to fix the M06 is to remove it in postbu...

Experimenter
Experimenter

The simplest way to fix the M06 is to remove it in postbuilder. Operation Start Sequence ->Auto Tool Change. In the Block with the Tnn drag the M06 to the trash can.

If this is a new post, beware of other things that may need fixing:

G04 should be non-modal and I force it to cancel the G04 with a custom command.

PB_CMD_cancel_dwell

MOM_force once G_motion

I put this in the Delay in Machine Control

 

Also change G94/G95 to G98/G99 for the feedrate modes if needed.

 

Learn online





Solution Information