Cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between Normal to Drive and Toward Dirve in multi axis ?

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

I do not know and How to use  Normal to Drive and  Toward Drive  ?

 

Thank .

4 REPLIES

Re: What is the difference between Normal to Drive and Toward Dirve in multi axis ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Normal to drive specifies that the projection is done normal to the drive geometry, this is not useful for machining the side walls of a closed pocket.

 

Toward drive was introduced to be able to machine the side walls of closed pockets.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: What is the difference between Normal to Drive and Toward Dirve in multi axis ?

Imagine machining inside of a large tube.

 

With normal to drive, the path projects from infinity and always lands on the outside of the tube. This is the traditional APT behavior.

 

With toward drive, we start at the surface and back away, allowing the path to project on to the inside of the tube. 

 

If there are no overhangs, and no eclosed areas, then both should yield the same result.

Mark Rief
Retired Siemens

Re: What is the difference between Normal to Drive and Toward Dirve in multi axis ?

Pioneer
Pioneer
In this case Tool Axis will be normal to drive?

Re: What is the difference between Normal to Drive and Toward Dirve in multi axis ?

Genius
Genius

No, these options are for projecting the tool path onto the part, not for controlling the tool axis.

Mike Diamond, CNC Programmer, Orizon Aerostructures Inc.

Production: NX10.0.3.5, Vericut 7.4.1, ICAM V21
Development: VB.NET, Tcl/Tk
Testing: NX11

Learn online





Solution Information