Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

What's the optimal hardware configuration for NX CAM?

Experimenter
Experimenter

 

Our config you can see below.

2 Intel Xeon E5-2667 3.3GHz

2 NVIDIA Quadro K5000

128 GB ram

Win7 64 bit

 

With this pc, the generating time at complex part is too long.

If i use a "floor and wall" for a simple surface milling, i pick the top face for floor, after that the programm is thinking for 2-3 minutes. So for example i want to change on containment page, the extend floor from thickness to part outline or blank outline. Okay i must wait another 3-4 minutes for work in process window. Next step the generating... Every time if i want to change something i wait for the processing and this was just a simple machining.

 

A simple laptop config like i7 4700MQ with 2 Nvidia 755M is better than the workstation??

Cause our measurements say this.

Laptop generating e.g. 10 minutes.

Workstation generating e.g. 15 minutes.

 

What's the optimal hardware configuration for NX CAM?

 

Thank you for your help.

4 REPLIES

Re: What's the optimal hardware configuration for NX CAM?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Disable the preview for floor/wall operations through the customer defaults.

Don't use FLOOR_WALL_IPW, if you don't need/have an IPW.

What NX release are you working with, there have been significant enhancements in NX 10.0.3 regarding floor/wall performance.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: What's the optimal hardware configuration for NX CAM?

Valued Contributor
Valued Contributor

https://support.industrysoftware.automation.siemens.com/certification/index.shtml

EDS UG V3 -UG V15 UNIX; UGS UG V6 -UG V19 - NX-NX5 UNIX/MS;
Siemens NX6-NX10; NX11; NX12; NX1847 MS

Re: What's the optimal hardware configuration for NX CAM?

Experimenter
Experimenter

Thanks for the fast reply Stefan Pendl.

 

That option solved the waiting time between two generate.

 

But the problem than NX just use 3% from the CPU capacity and 15% from the GPU capacity is standing yet.

 

Re: What's the optimal hardware configuration for NX CAM?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX CAM is constantly enhanced to support multi-threading when ever appropriate.

This will increase the usage of multiple cores in the near future.

If you use NX 10.0.3, you will find that there is a performance boost for multiple operation types compared to NX 8.5.3 when generating tool paths.

There are limitations due to the architecture of the tool path generation processor, so it is not always possible to improve all operations.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information