Cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the value of "ptp_file_name" set in post?

Valued Contributor
Valued Contributor

We use NXCAM with TC. In NX8.5 the output-path of the ptp-file was:

 

C:/TEMP/D1594417_1/ptp/nc_program/machine1_itnc530/D1594417_0.ptp

 

In NX10 the output-path of the ptp-file is:

 

C:/TEMP/D1594417__0____4/ptp/nc_program/machine1_itnc530/D1594417_0.ptp

 

The variable-name of this path should be "ptp_file_name". Where does it come from? I can't find a place where it is. Why is there a difference in NX10 between NX8.5?

 

I believe that's the reason, why it's not possible to debugg the post in NX10. Native the debugger works.

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk
5 REPLIES 5

Re: Where is the value of "ptp_file_name" set in post?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There's 2 (or more) variables used:

 global mom_output_file_full_name
 global ptp_file_name

 

You need to check/set both.  If they are not consistant, I would set ptp_file_name to be the same as mom_output_file_full_name.

 

The "temp" folder used by NX when running in TC is an NX/TC thing, set as the file is opened.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Where is the value of "ptp_file_name" set in post?

Valued Contributor
Valued Contributor

I don't set this global variables. They come from system automaticly.

Actually, to me the path name does not matter. I only thought, that this could be the reason, why the debugger is not running. Perhaps I'm wrong with it.

 

I want to know why debugger in TC-Environment is not running, also with one of your standard-posts, See Attachement. Nativ, without TC it is running.

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk

Re: Where is the value of "ptp_file_name" set in post?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have no problems running the debugger w/ TC2007 / NX7.5

I'd suggest reporting to GTAC

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Where is the value of "ptp_file_name" set in post?

You need to report this to GTAC.

 

It's possible something changed in how TC names temporary files, that is not known by the review tool.

Mark Rief
Retired Siemens

Re: Where is the value of "ptp_file_name" set in post?

Legend
Legend

I think the place where ptp_file_name is set is this:

...\Siemens\NX 10.0\MACH\resource\template_dir\cam_output.tcl

in particular you should check this proc

 

proc DBC_form_output_path

 

but i don't know if it can solve your debug problems.

 

hope it helps

ciao

luciano

 

Learn online





Solution Information