Cancel
Showing results for 
Search instead for 
Did you mean: 

Where to define UGII_CAM_CSE_USER_DIR

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hello everyone.

I've been facing a problem to define UGII_CAM_CSE_USER_DIR variable.

Because, in my setup, i put the post processor to write to_ini.ini in the ENV variable ( cse_driver\subprog\to_ini.ini), and i'm calling the file in the ini file from the part. and i have a question where i can define this variable.? ( in the .dat file, or en env.dat? 

 

 




2 REPLIES 2

Re: Where to define UGII_CAM_CSE_USER_DIR

You can define it in many ways, as long as it is defined before NX starts. I use a ugii_env.dat file in the start-in folder, but you could also use a .bat file or define it in Windows. If you are new to this, look at this video at the 08:15 mark. 

Mark Rief
Retired Siemens
Highlighted

Re: Where to define UGII_CAM_CSE_USER_DIR

Siemens Pioneer Siemens Pioneer
Siemens Pioneer
Hello @MarkRief . Thanks for your advice.
i just saw a little time ago. My specific problem was with where is the best plance, but now, everything are ok

Thanks for the fast answer.

WBR

Marco Antonio R. Silva
Siemens PG SU Brazil

Learn online





Solution Information