Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Which Java Version

Legend
Legend

Any Idea which version of Java mkes NX12 Help files happy?

 

Thanks in Advance, Paul S.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

6 REPLIES 6

Re: Which Java Version

Siemens Phenom Siemens Phenom
Siemens Phenom

I believe I am running jre1.8.0_72 

Re: Which Java Version

I am running 8-171 at the moment. To be honest I am not sure what the recommended java version is but I believe my doc server has all the current updates and is running great; no reports of any issues from our users.

NX 12.0.2

Re: Which Java Version

Legend
Legend

Thanks for the info. I know back on NX10 I had broken the system by jumping ahead in java versions, then had to uninstall and find an older version.

 

Paul S.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Which Java Version

Valued Contributor
Valued Contributor

We don't load/setup local helpfiles anymore.  We leave the doc location undefined at startup and NX defaults to the Siemenens web site with all the  docs.  Always up to date and matches the rev  and point rev you are running.

 

I asked many years ago when we had the JAVA problem in 8.x and I was told online docs would be supported for a "long time" after release.  

 

No one has complained yet about the response.

Re: Which Java Version

@VH
Thank you for the tip. I knew of online docs but I wasn't aware NX would access them directly. I deleted the UGII_UGDOC_BASE variable and it works great.
NX 12.0.2

Re: Which Java Version

Experimenter
Experimenter

jre1.8.0_72 is the best.

Learn online





Solution Information