Cancel
Showing results for 
Search instead for 
Did you mean: 

Why do I get error message " secondary rotary position being used "

Creator
Creator

I could be missing something, but I only see "I" & "K" vectors

 

I did roughing, then added mill control for stop & message, then next operation gives me error?

 

below is partial of list file of cutting

 

TOOL PATH/MACHINE_STOP_4,TOOL,4.00_X_45DEG_FACEMILL

TLDATA/MILL,4.7400,0.0000,0.7500,0.0000,0.0000

MSYS/0.0000,3.7030,0.0000,1.0000000,0.0000000,0.0000000,0.0000000,1.0000000,0.0000000

$$ centerline data

PAINT/PATH

PAINT/SPEED,10

LOAD/TOOL,1,ADJUST,1

COOLNT/OFF

INSERT/G28

STOP

DISPLY/ROTATE OR REPLACE INSERTS

COOLNT/FLOOD

PAINT/SPEED,10

PAINT/TOOL,NOMORE

END-OF-PATH

 

TOOL PATH/P_ROUGH_MAIN_FACE_TOP,TOOL,4.00_X_45DEG_FACEMILL

TLDATA/MILL,4.7400,0.0000,0.7500,0.0000,0.0000

MSYS/0.0000,3.7030,0.0000,1.0000000,0.0000000,0.0000000,0.0000000,1.0000000,0.0000000

$$ centerline data

PAINT/PATH

PAINT/SPEED,10

LOAD/TOOL,1,ADJUST,1

SPINDL/RPM,764,CLW

PAINT/COLOR,186

RAPID

GOTO/-66.7700,5.0527,-11.5456,-1.0000000,0.0000000,0.0000000

PAINT/COLOR,211

RAPID

GOTO/-51.7700,5.0527,-11.5456

PAINT/COLOR,6

FEDRAT/IPM,22.9200

GOTO/-51.7700,4.8835,-7.2830

PAINT/COLOR,31

GOTO/-51.7700,4.7855,-4.8163

 

below is partial of my .lpt file

 

X-4.7748Y6.917                               -4.7748    6.9170   47.9300 327.500  -0.000   22.9  764
Z48.03                                       -4.7748    6.9170   48.0300 327.500  -0.000   22.9  764
G00Z75.2387                                  -4.7748    6.9170   75.2387 327.500  -0.000  400.0  764
N167(MACHINE_STOP_2)
N168M09                                      -4.7748    6.9170   75.2387 327.500  -0.000  400.0    0
N169G28                                      -4.7748    6.9170   75.2387 327.500  -0.000  400.0    0
N170M00                                      -4.7748    6.9170   75.2387 327.500  -0.000  400.0    0
(ROTATE OR REPLACE INSERTS)
N171(ROTATE OR REPLACE INSERTS)
N172M08                                      -4.7748    6.9170   75.2387 327.500  -0.000  400.0    0
N173(G_ROUGH_MAIN_FACE_TOP)
N174S764M03                                  -4.7748    6.9170   75.2387 327.500  -0.000  400.0  764
secondary rotary position being used
N175G57H901                                 -11.5458    5.0465   66.7700  90.000  -0.000  400.0  764
N176G173W0.0                                -11.5458    5.0465   66.7700  90.000  -0.000  400.0  764
N177G00X-11.5458Y5.0465                     -11.5458    5.0465   66.7700  90.000  -0.000  400.0  764
N178G43Z66.77H001                           -11.5458    5.0465   66.7700  90.000  -0.000  400.0  764
B90.                                        -11.5458    5.0465   66.7700  90.000  -0.000  400.0  764
Z51.77                                      -11.5458    5.0465   51.7700  90.000  -0.000  400.0  764

1 REPLY

I think you might get an answer sooner if you log a call...

I think you might get an answer sooner if you log a call with GTAC. They can probably look at your post and the operations to see why the alternate position is being used.

Mark Rief
Retired Siemens

Learn online





Solution Information