Cancel
Showing results for 
Search instead for 
Did you mean: 

Work Offsets

Valued Contributor
Valued Contributor

Is there a way to make sure correct work offset is posted out it seems different posts handle differently and some give error messages and some output without issue, I want to make sure program is setup correctly before looking at posts. Issue is a problem when moving a job from one machine to another

 

Thanks 

Mike

NX 11.0.2.7
Win 7
1 REPLY

Re: Work Offsets

Fixture Offset 1 is correct for the machine's first offset - i.e. G54 for Fanuc. 

If you move to a machine that uses something else, you should get G54.1P1 or E1 or whatever is correct for that machine, 

Is this the question?

 

If you want to make sure the programmer does not use 0, you need to check that in the post.

Mark Rief
Retired Siemens

Learn online





Solution Information