Cancel
Showing results for 
Search instead for 
Did you mean: 

Wrap FaceMill CAM Operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

 

I need to wrap a CAM operation (Face Mill) to a curved surface.

Can anyone please advise the right way.

 

Thanks & Regards

Sandeep Chugh

Wrap CAM Operation.png

10 REPLIES

Re: Wrap FaceMill CAM Operation

Gears Phenom Gears Phenom
Gears Phenom

I dont know any native function for this.

I think "NX open" is the way.....

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Wrap FaceMill CAM Operation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is there a reason you can't program this as a variable axis operation?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Wrap FaceMill CAM Operation

Legend
Legend

You can use a multiaxis operation like variable contour? Pick the curved faces in the operation and use "Projection Vector"--> "Toward line" The line would be the centerline of the part. 

Glenn Balon
Production: NX 12.0.2 MP5 Primarily CAM

Re: Wrap FaceMill CAM Operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

 

Have tried all the options of Variable Contour Operation in Multi Axis but not able to achieve the results.

 

There was a post earlier:

WRAP NX CAM Operation to Cylinder -

https://community.plm.automation.siemens.com/t5/NX-CAM/WRAP-NX-CAM-Operation-to-Cylinder/

wherein same objective is shown achieved using user defined operation (UDOP)

 

http://www.youtube.com/watch?v=lBggBZmK-B0

 

Am attaching prt file if anyone can generate same as shown in video please..

 

Thanks

Sandeep Chugh

 

 

 

Re: Wrap FaceMill CAM Operation

Legend
Legend

Probably not exactly what you are looking for, but as a starting point I came up with this in the few minutes I had to play with it. Some issues with geometry caused spiking. 

 

 

Glenn Balon
Production: NX 12.0.2 MP5 Primarily CAM

Re: Wrap FaceMill CAM Operation

Phenom
Phenom

If the machine supports "Cylindrical Interpolation" (G07.1 on our machines)

It is possible with some post customisation to use planar mill operations to do this.

I am not sure if it is possible to get CSE to simulate this correctly.

As we mostly use this for engraving on the OD of parts in a simple mill turn, simulation has not been a priority.

Re: Wrap FaceMill CAM Operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Possible to share please??

Highlighted

Re: Wrap FaceMill CAM Operation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I liitle bit edit your prt-file and toolpath, add feedrates and spindle speed, not so important, and wrap your path. You can use tapered tool or you can use multi-level CAVITY MILL operation. See attached prt.

 

WRAP_AGAIN.png

Re: Wrap FaceMill CAM Operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Many Thanks

Learn online





Solution Information