Cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong Z coord after plane spatial

Experimenter
Experimenter

 

Hi there,

 

i sometimes have the problem, that when i pp multiple 5ax operation in one nc file in some operations i get a wrong Z coord from the pp. 

It seems that its is always the value of 10mm, like in this case. Line "4198" increases by 10 from the previous one for any reason ?!

 

Is someone aware of this problem and knows how to fix it? 

 

 

4195 PLANE SPATIAL SPA+0.0 SPB-52. SPC-90. TURN FMAX SEQ-
4196 L X43.258 Y17.584 Z114.668 FMAX
4197 L Z12.934 FMAX
4198 L Z22.934 M3 M8
4200 L Z13.134
4201 L Z12.934
4202 L Z9.934

 

i'm using NX 10.0.3.5

 

thanks in advance

wolfgang

3 REPLIES 3

Re: Wrong Z coord after plane spatial

Gears Phenom Gears Phenom
Gears Phenom

check if the mom_pos array is not overided by mom_mcs goto array (like for continuos tcpm machining)

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Wrong Z coord after plane spatial

Experimenter
Experimenter

How can i check this ? 

 

i do not use tcpm.

Re: Wrong Z coord after plane spatial

Gears Phenom Gears Phenom
Gears Phenom

I am not telling this is the problem. Could be.

 

Just try to find it.

I dont know how is your PP made.

 

set mom_pos(0) $mom_mcs_goto(0)

etc

or VMOV function

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information