Cancel
Showing results for 
Search instead for 
Did you mean: 

Z LEVEL 5AXIS PROBLEM

Legend
Legend

Hello guys,

At first sorry for my poor english.

I have some problems with nx 5 axis operations.I can create 5 axis process easily but output of nc codes not working smootly on machine.while programme working on machine,there are always happening a bit stopping movements again and again.This is affecting surface quality and machine time so much.I sent you a section of a mould and nc code output.the machine is dmg  hsc105 lineer.I cant understand what is the problem?I am not expert on 5axis machining and post processors.

 

I am waiting for your sugestions.thank you.

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com
20 REPLIES 20

Re: Z LEVEL 5AXIS PROBLEM

PLM World Member Creator PLM World Member Creator
PLM World Member Creator

Hello,

 

Have you tried using M120?

Re: Z LEVEL 5AXIS PROBLEM

Legend
Legend

I dont know affect of M120.

 

at this time I  use nx10.0.3.5 and ı am sending a video 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: Z LEVEL 5AXIS PROBLEM

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Use tool axis towards point to get rid of the B-axis movement, which should be better suited for the machine.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Z LEVEL 5AXIS PROBLEM

Legend
Legend

can u send me prt file with changes of tool axis.ı want to test it on machine.

if you see prt file ı want b axis 15 degree but output of nc codes there are a lot of b axis changes between 13-15 degree.why this is happening?why ı couldnt fix b axis.

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: Z LEVEL 5AXIS PROBLEM

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Attached find the edited part file, there should be one B axis change per level only.

Through point doesn't use a fixed tilted axis, but it keeps the tilt axis the same for one level.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Z LEVEL 5AXIS PROBLEM

Legend
Legend

I open prt file but tool axis still away from part,Stefan.I suppose u didnt do any changes.

is there a way create 5axis z level operation with fixed tool axis and get smooth tool path movements on machine.

 

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: Z LEVEL 5AXIS PROBLEM

Valued Contributor
Valued Contributor

Hello,

 

are you sure everything is correct with your post? Taking a look at the internal path (listing the toolpaht from the operation dialog) we can see that the z-component of the tool-axis vector is constant (0.9659258). This should cause a constant b-axis on an ortogonal kinematic like yours.

To test this i used one of my posts and got a constant tilt angle to the z-axis of 15 degrees.

 

In general i agree with stefan to use orientation toward point in this case, especially to get a smooth and continious movement of the c-axis. Furthermore i would use a far smaller in/out-tol to take into accont the small size of the tool. Your in/out-tol leeds to direction changes in the path up to 10 degrees between the single linear segment. Another effect is that you have changes of the c-axis up to 3 degrees from one nc-point to the next.

 

And check if there are any side effects while using CYCLE392 and CYCLE32 in one program. As far as i know CYCLE392 is a DMG cycle to control the dynamic of the machine. Maybe you have to use either 392 or 32. But I'm not sure at this point.

 

Regards,

 

Peter

 

Re: Z LEVEL 5AXIS PROBLEM

Legend
Legend

we dont use nx own post builder and ı am not expert on post processors.ı'm not sure my post processor right or false for that ı send nc codes if there is an error in my post processor.to tell the truth ı am in trouble with this and ı dont know what to do

 

 

 

 

 

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: Z LEVEL 5AXIS PROBLEM

Valued Contributor
Valued Contributor

is the posted nc-file exactly the ouput of your post for the operation in the provided nx-part?

Learn online





Solution Information