Cancel
Showing results for 
Search instead for 
Did you mean: 

ZLEVEL improvement "mixed with climb cut"

Pioneer
Pioneer

Now curruntly three cut direction available on zlevel operation ., 

climb ,conventional ,mixed 

 

i am saying to improve with more option like "mixed with climb cut " and improved over singal program stratrgy .

 

i am attached image for better understand .,image shows two diffrant pass , first was mixed cut and second was climb cut.

111.png

8 REPLIES

Re: ZLEVEL improvement "mixed with climb cut"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Patel,

 

I am not really sure if I can follow here. How should a mixed with Climb Cut work? 

 

If you want to have the result you are showing in the picture, your way of programming would be the one I would advise also.

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: ZLEVEL improvement "mixed with climb cut"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In this particular situation this would be similar to automatic inward or outward of cavity milling.

Mixed would be used for open walls and climb/conventional for closed walls.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: ZLEVEL improvement "mixed with climb cut"

Siemens Phenom Siemens Phenom
Siemens Phenom

If the consistence in surface quality doesn't matter, this would be a valid approach.

Lead Product Manager - Mold & Die

Re: ZLEVEL improvement "mixed with climb cut"

Pioneer
Pioneer

yes you ar right ,, i'm using this for semi-finish so dont matter for any surface finish...

 

what you say about?  @AlexanderFreund

Re: ZLEVEL improvement "mixed with climb cut"

Experimenter
Experimenter

hello patel.

 

why don't i have this option? im using nx12

Re: ZLEVEL improvement "mixed with climb cut"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Fischer_Dan,

 

I would advise our Area Mill Steep Zlevel Zig Zag Cut Pattern for the upper part of this geometry (Picture1). Additionally we will release Area Mill Helical in NX12.0.2 by tomorrow (Picture 2). This pattern should be first choice for pockets. The Area Mill operation will give you a superior surface finish.

Zig_Zag.pngPicture 1 - ZLevel Zig Zag

Helical.pngPicture 2 - ZLevel Helical

2018-07-16 12_21_19-NX 1847.1500 _ CAM_nx1847.213 - Manufacturing.png

 

 

You can easily define your regions with the Cut Region Manager.

 

Cheers,

Alexander

 

Lead Product Manager - Mold & Die

Re: ZLEVEL improvement "mixed with climb cut"

Experimenter
Experimenter

thanx alexander, cant find these operations, im using nx 12.0.0.27

Re: ZLEVEL improvement "mixed with climb cut"

Siemens Phenom Siemens Phenom
Siemens Phenom

My suggested workflow is in Area Milling, also available in NX12:

Area_Milling.pngArea Milling - Cut Region Manager (CRM)Contour_Area_template.pngContour Area Template

Lead Product Manager - Mold & Die

Learn online





Solution Information