Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

area milling

Pioneer
Pioneer

rampa.jpg

 

how to let the tool path like the image because when I machining it recognizes the hole

3 REPLIES 3

Re: area milling

Some operations have options to cross the gaps.

  • Cutting Parameters > Connections > Across Voids

In general, you need to remove the hole so that the CAM operation does not see it. There are many ways, depending on how your assembly is organized 

  • If you own the model supress the hole feature
  • Use Synchronous to cover the hole
  • In an assembly, Wave link the body, then use Synchronous modeleing to cover the hole
  • In an assembly, Wave link the body at a timestamp before the hole

I'm sure there are more ...

 

Mark Rief
Retired Siemens

Re: area milling

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
Fixed contour > drive:surface area > select face > no part geometry
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: area milling

Experimenter
Experimenter

1f9d1943a72da9657aa7f03caba42234.png2c650a59eaa9313984bfbcf6fbe98937.png

 6e89a72085d8cc9a74c548c4de09c4f1.png

i use the other  3 ways to solve  your problem 

u can download the prt to see the detailed 

the surface is steep  , i recommedate to use zlevel  

 

Learn online





Solution Information