Cancel
Showing results for 
Search instead for 
Did you mean: 

cam_part_planner_library.dat and Tool Axis (create operation)

Legend
Legend

If I open  Manufacturing in Teamcenter managed mode where cam_part_planner_library.dat config is used, there is another dialog shown without Tool Axis menu.

 

If I work in native NX without PDM and cam_general.dat configuration is used then Tool Axis menu is presend.

See two screenshots below

 

How to set Tool Axis in manufactuing in teamcenter mode?

3 REPLIES 3

Re: cam_part_planner_library.dat and Tool Axis (create operation)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Those do not look like the normal "as installed" dialogs.

It could be you are using 2 different OPT files, or 2 different operation template parts?

 

Or it could be a bug / "feature" :-(

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: cam_part_planner_library.dat and Tool Axis (create operation)

The templates in teamcenter are many years out of date. Import the CAM templates from your NX instalation.

Mark Rief
Retired Siemens

Re: cam_part_planner_library.dat and Tool Axis (create operation)

Legend
Legend

Yes, you are right!

I imported NX10 CAM templates with tcin_cam_template_setup and all became fine

Learn online





Solution Information