Cancel
Showing results for 
Search instead for 
Did you mean: 

cavity mill

Pioneer
Pioneer

colisao.jpg

 

 

 

 

YOU MIGHT ME WITH THIS PROBLEM Help No Cavity MILL IT IS INVADING WALL am nx User 8.5 Thank you very much in advance CLAUDIO csouzabira@gmail.com

2 REPLIES 2

Re: cavity mill

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello that might be a tolerance problem of verify, when the cutting portion and the shaft has exactly the same diameter. To get evidence about that you could try to make the shaft a 0.1 mm smaller.

 

Since 903 MP2 we store the IPW settings with the part file (CAM Preferences) here it is also possible to change the chordal tolerance which influence the faceting of the tool and can solve such tolerance topics.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: cavity mill

Pioneer
Pioneer
I changed the diameter

the tool shank and it worked

thank you!!!!

Claudio

Learn online





Solution Information