Cancel
Showing results for 
Search instead for 
Did you mean: 

clearance height of hole making drill

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi

 

NX Version is 11.0.2

I have a question regarding the clearance movement of the hole making drill.

I have set clearance options to "none" and set between Fature to "direct".

And collision check to off.

However, it is generated with an unknown clearance height value.

 

Hole_making.jpg

The equipment uses a cycle code, so it can be moved directly.

Is there a changeable way?

 

 

1 REPLY

Re: clearance height of hole making drill

Siemens Genius Siemens Genius
Siemens Genius

You have defined a direct transfer between features but this direct transfer will only be applied when the tool axis difference between subsequent features is within 0.1 range. Increase your max tool axis change to 90 degrees to have the direct transfer applied.

 

Thanks,

 

Toon van der Kooi

 

 

Learn online





Solution Information