Cancel
Showing results for 
Search instead for 
Did you mean: 

corner value problem

Valued Contributor
Valued Contributor

I created some different type operations with corner radius and got different results.I sent some jpg files and prt data.

What affects corner radius value?  

-----------------------------------------
NX 11.0.2.7 MP10 / Testing NX 12.0.2.9
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com
2 REPLIES

Re: corner value problem

In the zlevel 5MM, the radius is being limited by the stepover limit. Raise the limit to 300% and you will get your 5 mm radius. This is to limit the amount of material left in the corners or between passes.

In the area milling steep, it should and just like Zlevel, but it looks like the radius is reduced to assure cleanup in the corner. I'm not sure where the 1mm radius is from. 

Mark Rief
Retired Siemens

Re: corner value problem

Valued Contributor
Valued Contributor

thanks mark for your reply.I missed stepover limit factor.

-----------------------------------------
NX 11.0.2.7 MP10 / Testing NX 12.0.2.9
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Learn online





Solution Information