Cancel
Showing results for 
Search instead for 
Did you mean: 

custom error message....

Pioneer
Pioneer

Hello,

 

I was wondering if there is a way to create a popup window that I could use as a kind of custom error message for the user.  For example,

 

if {maxSpindle < 0} {

      pop-up window "go to line 33 of source file to debug"

}

 

Is there a simple text widget command than I can use?

1 REPLY 1

Re: custom error message....

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

starting from NX9, we can use:

 

MOM_display_message

 

Displays OK button if no label specified, and returns 1

 

MOM_display_message <message> <title> <type> [<button1>][<button2>][<button3>]

 

Displays a message dialog box in NX. <type> is the style of the message box, I|E|W|Q, where I is info, E is error, W is warning, and Q is question. Button labels are optional. Returns the number of the button (1, 2, or 3) that the user clicks.

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Learn online





Solution Information