Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

cycle off

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

2018-06-14_1045.pngHello, As the image above two drill cycle separated by cycle off. How to generate it likes.... 

 

CYCLE/DRILL,xxxxxxxx

GOTO XXXXXXX      (position of first hole)

GOTO XXXXXXX      (position of second hole)

CYCLE/OFF

 

 

3 REPLIES 3

Re: cycle off

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Holemaking or legacy PTP?

Do you have a clearance plane or "avoid" or "retract to" (or ?) defined?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: cycle off

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I use hole making. 

2018-06-15_0833.png

Re: cycle off

Siemens Legend Siemens Legend
Siemens Legend

For drilling the Retract Output Mode specifies when the retract level can be embed within the canned cycle mode.

 

Set this mode to Always (embed) to avoid cycle off for subsequent control points with equal tool axis orientation.

 

Note that the retract level differs between the two point ...

 

Learn online





Solution Information