Cancel
Showing results for 
Search instead for 
Did you mean: 

cylindrical interpolation G07.1

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

progrsmming a slot on the od of s part on a samsung sl25mc lathe

starting point is at c-90  (line N10480) at N10540 it's suppose to only go .4664 degrees but on

distance to go show 425 degrees to go anyone see what the problem is

 

 

 

 

(FINISH MILL SLOT)
N10430 M45
N10440 M69
N10450 G00 T0808 M08
N10460 G97 S3057 M13
N10470 G98
N10480 G19 X9.8 Z3.0 C-90
N10490 Z.7625
N10500 X9.255
N10510 G1 X9.125 F25.
N10520 G07.1 C4.5625
N10530 G1Z.7781 F1.6
N10540 C-90.4664
N10550 G2 Z.7625 C-90.6604 R.0625
N10560 G2 Z.7469 C-90.4664 R.0625
N10570 G1 C-89.5336
N10580 G2 Z.7625 C-89.3395 R.0625
N10590 G2 Z.7781 C-89.5336 R.0625
N10600 G1 C-90.0
N10610 G1 Z.7625
N10620 G07.1 C0
N10630 G1 X9.025 F25.
N10640 G07.1 C4.5125 (2ND DEPTH)
N10650 G1Z.7781 F1.6
N10660 C-90.4664
N10670 G2 Z.7625 C-90.6604 R.0625
N10680 G2 Z.7469 C-90.4664 R.0625
N10690 G1 C-89.5336
N10700 G2 Z.7625 C-89.3395 R.0625
N10710 G2 Z.7781 C-89.5336 R.0625
N10720 G1 C-90.0
N10730 G1 Z.7625
N10740 G07.1 C0
N10750 G00 X9.8
N10760 G0 Z3.5 M9
N10770 G99
N10780 G28 U0.0 W0.0
N10790 M30

4 REPLIES 4

Re: cylindrical interpolation G07.1

Phenom
Phenom

 

 

I dont have access to a Fanuc? manual at the moment.

However if G07.1 is like polar.

C is a virtual Y axis and dependant on the radius X?

 

How are you generating this output?

 

Guessing, probably need more info

Re: cylindrical interpolation G07.1

Phenom
Phenom

 

For G07.1 C is not a virtual Y as I thought.

Re: cylindrical interpolation G07.1

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

not according to the manual it breaks down the c axis into angular degrees this is a samsung mc25 with fanuc controller.  i want a small groove about .5 degrees of rotation -90 to -90.4664 but it gos 425 degrees.

Re: cylindrical interpolation G07.1

Phenom
Phenom

Sorry, I was talking about virtual axis like G12.1 Polar where is C a virtual Y value and the control calculates the angle.

 

As I read it G07.1 C is the angle.

G07.1.PNG

 

Have you tried to make all the C values positive?

 

(FINISH MILL SLOT)
N10430 M45
N10440 M69
N10450 G00 T0808 M08
N10460 G97 S3057 M13
N10470 G98
N10480 G19 X9.8 Z3. C270.
N10490 Z.7625
N10500 X9.255
N10510 G1 X9.125 F25.
N10520 G07.1 C4.5625
N10530 G1 Z.7781 F1.6
N10540 C-90.4664
N10550 G2 Z.7625 C269.3396 R.0625
N10560 G2 Z.7469 C269.5336 R.0625
N10570 G1 C270.4664
N10580 G2 Z.7625 C270.6605 R.0625
N10590 G2 Z.7781 C270.4664 R.0625
N10600 G1 C270.
N10610 G1 Z.7625
N10620 G07.1 C0
N10630 G1 X9.025 F25.
N10640 G07.1 C4.5125 (2ND DEPTH)
N10650 G1Z.7781 F1.6
N10660 C-90.4664
N10670 G2 Z.7625 C269.3396 R.0625
N10680 G2 Z.7469 C269.5336 R.0625
N10690 G1 C270.4664
N10700 G2 Z.7625 C270.6605 R.0625
N10710 G2 Z.7781 C270.4664 R.0625
N10720 G1 C270.
N10730 G1 Z.7625
N10740 G07.1 C0
N10750 G00 X9.8
N10760 G0 Z3.5 M9
N10770 G99
N10780 G28 U0.0 W0.0
N10790 M30

 

Learn online





Solution Information