Cancel
Showing results for 
Search instead for 
Did you mean: 

drill cyclee sort to remove backlash

Valued Contributor
Valued Contributor

Is there any way without a UDE to get in to use the same x and y approach direction when drilling holes to remove any backlash in the machine?

 

before drilling each hole move to its location using the x+ and y+ direction.  it would have to position to the opp side then move to final location.

 

i have over 500 holes to drill on this part.

 

thanks

 

Damian Forsythe
Impact Manufacturing Group
NX 10.0.3.5
3 REPLIES 3

Re: drill cyclee sort to remove backlash

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you want to have the post *always* do this, you can code it in the post (check mom_prev_pos, or else just hard code the move to X- Y- then back to X+ Y+)

 

Otherwse you'll need a UDE to tell the post when to (or not to) do this.

 

Does your machine have a G code to do this?  (some do, I think something like G60)

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: drill cyclee sort to remove backlash

Valued Contributor
Valued Contributor

Thanks Ken.  yes the machine has G60, but in the manual, its says not recomened for this controle ( haas ).  i will try to find out what they mean by that.

 

Thanks

Damian Forsythe
Impact Manufacturing Group
NX 10.0.3.5

Re: drill cyclee sort to remove backlash

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I didn't see the word "sort" in your title.

Note there are some methods to sort holes in some sort of order, but *in general* one of the axes will have to reverse (i.e. you can alway position from greater to lesser X, but then the Y may be going up & down.)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information