Cancel
Showing results for 
Search instead for 
Did you mean: 

drilling depth setting

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I have a question on the drill.

 

I would like to set the depth value based on Tool Tip.

But it is set based on CL_SHOULDER.

 

TTT.jpg

 

Is there a way?

3 REPLIES

Re: drilling depth setting

Legend
Legend

I don't think so, You can still use the old school drilling which has that option

 

The tip length is described on the tool page.

Just have to do the math

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: drilling depth setting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Do not change the depth of the hole feature, since that doesn't capture the intent of the user.

It is much better and easier to use the setting "use predefined depth", which works much better and more reliable for manual changes.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: drilling depth setting

Pioneer
Pioneer

Hi,

 

1-Change tool drive point to SYS_CL_TIP.

2-Let you refresh with "reorder list".

hole.JPG

Learn online





Solution Information