Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

getCollJointValue and Synchronization Manager

Genius
Genius

I am having trouble using Synchronization Manager.  I have an operation that posts a subprogram named TEST.  Inside that subprogram is the anycontroller command getCollJointValue shown below:

 

##LANGUAGE AC
    FLOAT fColValueF1;
    fColValueF1 = getCollJointValue("F1", 35, "Table_Parts", "SETUP1");
##LANGUAGE NATIVE

I can post and simulate this operation on its own and with other operations in the same channel.

 

When I try posting or simulating with other channels, and the synchronization manager opens, it crashes the manufacturing environment. The issue seems to be the getCollJointValue line, because I can comment that out and it works.  

 

Any idea what's going on here?

 

 

Thank you.

3 REPLIES 3

Re: getCollJointValue and Synchronization Manager

Legend
Legend
If you use SyncManager and have more Channels use

getCollJointValueCh (<RefChannelName>, <strJointName>, <dTargetJointValue>[, <strSelectionType>, <strSelectionIdentifier>])

getCollJointValueCh ("1", "F1",35, "Table_Parts", "SETUP1");

Re: getCollJointValue and Synchronization Manager

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Jesse,

 

sorry, that you run into that problem. We found that too shortly.

As a fast way of continue I suggest to works with SetStopAtCollision instead of getCollJointValue.

IF you need some help let  me know

A fix of the initial core problem in on his way.

 

PS: Simulation should work, but starting Synch-Manager will fail.

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: getCollJointValue and Synchronization Manager

Genius
Genius

schauerm3: unfortunately that didn't seem to solve it for me.

 

Thomas:  That worked, thank you.  Certainly a more involved solution.  Any idea when getCollJointValue will work with sync manager?

Learn online





Solution Information