Cancel
Showing results for 
Search instead for 
Did you mean: 

helical milling, arc to linear output-CLSF source

Creator
Creator

Hi,

 

my name is Alex and I have a question regarding CLSF source output. I have tried to find such topic, but I did not succeed.

I would like to ask you guys, how to make CLSF output GOTO's instead of CIRCLE. I would like my post-processor to generate G01 and not G02/G03 in the helical milling cycle. Would someone be willing to show me how to do this?

I tried to modify    pb_cmd_helix - set mom_kin_helical_arc_output_mode LINEAR   MOM_reload_kinematics 

but that did not do anything. Is this only for post_processor and not for CLSF output?

Thank you very much and have a great day!

 

Regards

 

Alex

 

6 REPLIES

Re: helical milling, arc to linear output-CLSF source

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As the CLSF uses something similar to "turbo" mode in NXPost, I'm not sure ths is possible (Someone with more knowledge, likely from Siemens, would need to answer)

 

Note you CAN control this in your NX operations.

If you are using the "as installed" dialogs, under the "Machine control" block is a setting "Motion output type"

Set that to "Line" and you will only gte linear moves.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: helical milling, arc to linear output-CLSF source

Creator
Creator

Unfortunately when helical milling is used that option is not there. I cannot change Motion Output Type to Line.

Re: helical milling, arc to linear output-CLSF source

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

You could use Planar Mill with a helical engage.

Re: helical milling, arc to linear output-CLSF source

Gears Phenom Gears Phenom
Gears Phenom

You can customize the Hole Milling dialog and add the Motion Output Type to the dialog.

 

output-type.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: helical milling, arc to linear output-CLSF source

Creator
Creator

Hello,

 

thank you for your help. I have tried it, unfortunately it has not helped. It does not do anything.

Thank you anyway.

 

Alex

Re: helical milling, arc to linear output-CLSF source

Creator
Creator

Hi,

 

it is me again. I've tested ti again and it works. It has not done it properly the first time.

 

Big thank you, sir!

 

Best regards

 

Ales

Learn online





Solution Information