Cancel
Showing results for 
Search instead for 
Did you mean: 

how to change non parametric to parametic in nx

Experimenter
Experimenter
 
1 REPLY 1

Re: how to change non parametric to parametic in nx

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

How did you get a non-parametric part?

Import STEP or Parasolid or whatever?

Or did someone take an NX parametric part and "remove parameters"?

 

In any case, if you want a parametric model, you will (pretty much) either:

- Have to re-model from scratch

- Just use "synchronous modeling" techniques to modify the non-parametric solid as needed

- (if someone had a parametric model, you could ask for that instead of the de-parameterized model)

 

Note FBM should work just fine without a parametric part, unless you have a lot of FBM rules that depend on parameters / surface finishes / etc. (that didn't make it across to the part you have...)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information