Cancel
Showing results for 
Search instead for 
Did you mean: 

how to machine slot without variable contour

Pioneer
Pioneer

Hi

in part i need to machine 28 slots (r2+r25 in the middle) with movement of 4th axes. i dont have variable contour.

machining on vertical machine on 4th axis.

i need only 1 slot and then rotate.

thank you all for help.

p.s: nx 10 or 11..

3 REPLIES 3

Re: how to machine slot without variable contour

Siemens Phenom Siemens Phenom
Siemens Phenom

Hey @mor5789,

 

attached is the programmed part file. As you said, I only programmed one slot, because I guess you do the instances and rotation on the machine and calling the program again.

 

I would wish you had NX12.0.2, because than you could utilize our new Area Mill Spiral, which is the choice to go for such a symmetric geometry (see picture below).

Area_Mil_Spiral.pngArea Mill Spiral

I attached both, an NX11 and NX12 version.

 

Let me know if this fits for you.


Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: how to machine slot without variable contour

Pioneer
Pioneer

Hi

your moves are just perfect.

is it possible to do move with 4th axis?

 

thank's

 

Amnon

Re: how to machine slot without variable contour

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes of course. The program I made is just 3-Axis Toolpaths.

 

I think you can just do the rotation on your machine and call the programm again.

Lead Product Manager - Mold & Die

Learn online





Solution Information